DIN#.FILTER

Description

This parameter gets or sets the digital input filter. The digital filter blocks input changes (rising or falling edges) until the minimum pulse width is exceeded. The +/- tolerance listed is the sample period (uncertainty) of the filter.

Value Description Min PulseClosed When the step gets activated, the action is activated for a single execution, and possibly once again when the step is deactivated Width Typical Use
0 Unfiltered >40ns RS485 inputs
4 Ultra fast

>240ns

+/- 40ns

Fast Optos

1 Fast

>10.24 µs

+/- 0.64 µs

Fast Optos
2 Standard

>163µs

+/- 10.24µs

Slow Optos
3 Slow

>2.62ms

+/- 0.16384ms

Mechanical switch

Examples

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 4
Default Value

Depends on DIN:

4 for DIN1-2

2 for DIN3-12

Data Type Integer
See Also  

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

DIN1.FILTER

3590h

02h

Unsigned8

-

-

Read/Write

No

DIN2.FILTER

3591h

02h

Unsigned8

-

-

Read/Write

No

DIN3.FILTER

3592h

02h

Unsigned8

-

-

Read/Write

No

DIN4.FILTER

3593h

02h

Unsigned8

-

-

Read/Write

No

DIN5.FILTER

3594h

02h

Unsigned8

-

-

Read/Write

No

DIN6.FILTER

3595h

02h

Unsigned8

-

-

Read/Write

No

DIN7.FILTER

3596h

02h

Unsigned8

-

-

Read/Write

No

DIN8.FILTER

3597h

02h

Unsigned8

-

-

Read/Write

No

DIN9.FILTER

3598h

02h

Unsigned8

-

-

Read/Write

No

DIN10.FILTER

3599h

02h

Unsigned8

-

-

Read/Write

No

DIN11.FILTER

359ah

02h

Unsigned8

-

-

Read/Write

No

DIN12.FILTER

359bh

02h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DIN1.FILTER

20100

4E84

Unsigned8

Read/Write

-

DIN2.FILTER

20101

4E85

Unsigned8

Read/Write

-

DIN3.FILTER

20102

4E86

Unsigned8

Read/Write

-

DIN4.FILTER

20103

4E87

Unsigned8

Read/Write

-

DIN5.FILTER

20104

4E88

Unsigned8

Read/Write

-

DIN6.FILTER

20105

4E89

Unsigned8

Read/Write

-

DIN7.FILTER

20106

4E8A

Unsigned8

Read/Write

-

DIN8.FILTER

20107

4E8B

Unsigned8

Read/Write

-

DIN9.FILTER

20108

4E8C

Unsigned8

Read/Write

-

DIN10.FILTER

20109

4E8D

Unsigned8

Read/Write

-

DIN11.FILTER

20110

4E8E

Unsigned8

Read/Write

-

DIN12.FILTER

20111

4E8F

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DIN1.FILTER

20100

Unsigned8

Read/Write

-

DIN2.FILTER

20101

Unsigned8

Read/Write

-

DIN3.FILTER

20102

Unsigned8

Read/Write

-

DIN4.FILTER

20103

Unsigned8

Read/Write

-

DIN5.FILTER

20104

Unsigned8

Read/Write

-

DIN6.FILTER

20105

Unsigned8

Read/Write

-

DIN7.FILTER

20106

Unsigned8

Read/Write

-

DIN8.FILTER

20107

Unsigned8

Read/Write

-

DIN9.FILTER

20108

Unsigned8

Read/Write

-

DIN10.FILTER

20109

Unsigned8

Read/Write

-

DIN11.FILTER

20110

Unsigned8

Read/Write

-

DIN12.FILTER

20111

Unsigned8

Read/Write

-